New Toolpanel System from item – Always have the right tool close to hand

The new Toolpanel System from item creates order at the work bench. Using Groove Plate Profile 8, users can arrange their tools clearly across a total of 19 system grooves. The flat design ensures easy integration into existing work benches and offers plenty of space for accessories on the front and back. Groove Plate Profile is 400 mm high and weighs just 5.2 kg per metre, making it easy to fit to any work bench. It can also be mounted on material supply trolleys and Pivot Arms. The various elements in the item Hook and Holder System bring additional flexibility to assembly workstations and are also incredibly simple to fit in place. They ensure that ratchet spanners, screwdrivers and tool bits can all be set down in seconds. Holders are fitted to the panel simply by inserting them into a groove and turning them 90° to lock them in place, ready for use. Removing and repositioning the holders is just as easy. As well as helping to organise a whole range of tools, the new system can also be used to mount documents and semi-open fronted boxes. Of course, compatibility with the Line 8 system groove means all existing products in the Hook and Holder System, Shelves and other custom fixtures can be attached with the greatest of ease. The Toolpanel System brings an additional component to the item MB Building Kit System that supports efficient and ergonomic work bench configuration.

item Industrietechnik GmbH

item Industrietechnik GmbH is a global market leader in building kit systems for industrial applications. It has been designing and marketing construction solutions for machinery, fixtures and plants since 1976. The product portfolio comprises more than 3,500 high-quality components designed for use in machine bases, work benches, automation solutions and lean production applications. Thanks to the inclusion of transport solutions and dynamic elements, the company’s products can cover virtually all working processes, from manual production to automated manufacturing. Around 500 highly skilled employees are involved in developing innovative solutions for state-of-the-art mechanical engineering and offer outstanding advice and support. item Industrietechnik GmbH is headquartered in Solingen, Germany. Eleven branches and support centres ensure the company is always close to customers in Germany. The group has wholly owned subsidiaries in the USA, China, Italy, Poland and Switzerland.

Company contact  

Nicole Hezinger • item Industrietechnik GmbH

Friedenstrasse 107-109 • 42699 Solingen • Germany

Tel.: +49 212 65 80 5188 • Fax: +49 212 65 80 310

E-mail: [email protected] • Internet: www.item24.com

Press contact

Rebecca Schmortte • additiv pr GmbH & Co. KG

Press work for logistics, steel, industrial goods and IT

Herzog-Adolf-Strasse 3 • 56410 Montabaur • Germany

Tel.: (+49) 26 02-95 09 92 4 • Fax: (+49) 26 02-95 09 91 7

E-mail: [email protected] • Internet: www.additiv-pr.de